首页 > 热门关键词 > WIFI天线
综合排序 价格 销量
-
符合条件商品:共730
图片
关键参数
描述
价格(含税)
库存
操作
5.1GHz至5.9 GHz, 8 dBi,宽频平板天线, 集成SMA母头连接器 - HG5158P 该低成本紧凑型平板室内广角WiFi天线是在5.8GHzUNII和ISM频段应用的理想选择。
  • 1+

    ¥1496.85
  • 200+

    ¥597.26
  • 500+

    ¥577.3
  • 1000+

    ¥567.44
  • 订货
  • 2.4 GHz 12 dBi八木天线 - 12英寸N型母头连接器 - HG2412Y-NF 卓越性能
    HyperGain HG2412Y带天线罩的八木WiFi天线具有高增益和45°的波束宽度。它还特别适合定向和多点IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?、公共无线热点应用和使用2.4GHz ISM频段的其他系统。此款天线采用独特设计,可以按垂直或水平极性安装。

    坚固且防风雨
    此款WiFi天线封在具有标准防火等级的抗紫外线天线罩中,可以全天候运行。HG2412Y天线附带一个可以倾斜和旋转60度的天线杆安装套件。

    定制连接器
    如果需要此款天线的定制连接器,请向销售人员咨询连接器选件、价格和供货情况。
    • 1+

      ¥1538.48
    • 200+

      ¥613.87
    • 500+

      ¥593.36
    • 1000+

      ¥583.22
  • 订货
  • 2.4 GHz 12 dBi八木天线 – 12英寸N型公头连接器 - HG2412Y-NM 卓越性能
    HyperGain HG2412Y带天线罩的八木WiFi天线具有高增益和45°的波束宽度。它还特别适合定向和多点IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?、公共无线热点应用和使用2.4GHz ISM频段的其他系统。此款天线采用独特设计,可以按垂直或水平极性安装。

    坚固且防风雨
    此款WiFi天线封在具有标准防火等级的抗紫外线天线罩中,可以全天候运行。HG2412Y天线附带一个可以倾斜和旋转60度的天线杆安装套件。
    • 1+

      ¥1553.46
    • 200+

      ¥619.84
    • 500+

      ¥599.13
    • 1000+

      ¥588.9
  • 订货
  • 2.6 GHz MMDS 8.5 dBi全向无线局域网天线 - HG2609U 高性能

    HyperGain HG2609U是专门用于2.6GHz MMDS频段的高性能全向WiFi天线。这款轻巧型天线兼容IEEE 802.16、802.20和WiMAX应用以及NLOS应用。The HG2609U is ideal for Wireless Internet Service Providers (WISP) offering service in the less crowded 2.6GHz band and is compatible with Navini? Ripwave?.

    > All Weather Operation

    Constructed for all weather operation, the HG2609U features sealed collinear brass elements inside a durable UV-stable machine gray fiberglass radome.排气端盖和底座内的排水孔可以防止湿气在天线内部积聚。由于具有这些特点,HG2609U可以在上方或下方安装。
    • 1+

      ¥1614.28
    • 200+

      ¥644.11
    • 500+

      ¥622.59
    • 1000+

      ¥611.95
  • 订货
  • 698~960/1710~2700MHz低PIM级交叉极化DAS板状天线 - N型母头 - HG72708XWPPR-NF The HyperLink HG72708XWPPR-NF is a low PIM rated, high performance directional wall mount MIMO panel antenna specifically designed for in-building wireless networks such as DAS (Distributed Antenna Systems) which are used to distribute Cellular and WiFi signals throughout a building or area. The Multi-Band design of this antenna eliminates the need to purchase different antennas for each frequency. This simplifies installations since the same antenna can be used for a wide array of in-building wireless applications where wide coverage is desired.

    Cross Polarized

    The HG72708XWPPR-NF features two independent antennas with cross polarization. This feature doubles the wireless capacity over the same channels. The antenna is fed via two plenum rated antenna leads terminated with N-Female connectors. One for +45° polarized and one for -45° polarized signals. This feature makes these antennas ideal for polarization diversity systems.

    Low PIM Rated

    The key to providing the best performance in a DAS application is to ensure the components used are low PIM rated. This helps meet the increasing demand for higher data rates and the ability to provide streaming video for mobile devices. With a low PIM rating of <-150 dBc, the HG72705CU-PR helps meets the most demanding PIM requirements for LTE/4G bands.

    The HG72708XWPPR-NG is designed specifically for in-building operation and is ideal for use in large open areas such as indoor courtyards, i
    • 1+

      ¥1653.42
    • 200+

      ¥1552.89
    • 500+

      ¥1501
    • 1000+

      ¥1475.36
  • 订货
  • NULL L-com的HG65807XPPR-NF为一款低PIM级高性能壁挂式安装全向天线,专门设计用于DAS(分布式天线系统)等楼内无线网络。L-com的HG65807XPPR-NF增益为5.5~7dBi,可用于在整栋楼内或整个区域内分布蜂窝信号和WiFi信号。HG65807XPPR-NF的工作频率为617~6000MHz,极其适合于包括LoRA、LTE-M及NB-IOT在内的5G、 LTE、CDMA、LPWAN/IoT/M2M应用。HG65807XPPR-NF天线的多频段设计使得单个天线能够满足多种需要宽覆盖的楼内无线用途需求,从而实现免于为每一频率分别购置不同的天线且使得安装更为简单的优点。 L-com的HG65807XPPR-NF具有60度方图,具有+/- 45倾斜极化,并具有N型连接器。并且采用N型连接器。在电信行业中,实现最佳性能的关键一点在于,确保所使用的部件为低PIM级部件。这一点有助于满足日益增长的高数据速率需求,以及移动设备的视频串流需求。HG65807XPPR-NF的工作频率为617~6000MHz,额定PIM低至<-150dBc,有助于满足5G与LTE/4G频段最为严苛的PIM要求。 L-com的HG65807XPPR-NF天线配置N型连接器,专门设计用于楼内使用,极其适合于室内庭院、室内运动场馆、会议中心及购物中心等大型开放区域。随附的安装支架与五金零件使得天线的安装极为简单易行。与L-com种类繁多的其他优质射频产品一样,该款5G蜂窝天线可在订购当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持与销售人员。
    • 1+

      ¥1662.59
    • 200+

      ¥663.39
    • 500+

      ¥641.22
    • 1000+

      ¥630.27
  • 订货
  • NULL L-com LCANLP1015是一款高性能宽带对数周期天线,设计用于698至6000 MHz的点对点通信。L-com的LCANLP1015具有11 dBi的增益,可用于宽频率范围内的远距离定向通信。LCANLP1015是提升5G、LTE、CMDA、LoRA、物联网和WIFI的理想选择。 对数周期天线LCANLP1015具有垂直波束宽度为50度,水平波束宽度为65度。该天线具有垂直极化,附带的安装支架允许垂直或水平安装配置。对数周期天线用作现有蜂窝信号较弱且需要达到更远距离情形中的放大器。L-com定向天线有一根8英寸长的预剥连接线,端接1个N型母头连接器。 L-com的698至6000 MHz对数周期LCANLP1015天线具有11 dBi的最大增益,适用于5G DAS网络,使用频段为:n1、n2、n3、n5、n7、n8、n12、n13、n14、n18、n20、n25、n26、n28、n29、n30、n34、n38、n39、n40、n41、n46、n47、n48、n53、n65、n66、n67、n67、n70、n71、n77、n78、n79、n80、n81、n82、n83、n84、n41、n96、n98、n95、n95、n95、n95、n91、n95、n95、n91、n91、n91、n91、n95、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、N。该款带有 N 型母头连接器的 5G 定向对数周期天线有现货,可在当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持和销售人员,他们将为您热情解答。
    • 1+

      ¥1667.57
    • 200+

      ¥665.37
    • 500+

      ¥643.14
    • 1000+

      ¥632.15
  • 订货
  • NULL L-com的LCANLP1003为一款高性能的宽带对数周期天线,设计用于617~2700MHz点对点通信。L-com的LCANLP1003天线具有11dBi的增益,可用于极宽频率范围内的长距离定向通信。LCANLP1003天线极其适合用于5G、LTE、CMDA、LoRA、IoT、WIFI的放大。 LCANLP1003对数周期天线的垂直波束宽度为50度,水平波束宽度为75度。该款天线为垂直极化天线,随附的安装支架既允许安装为垂直构型,也允许安装为水平构型。对数周期天线用作现有蜂窝信号较弱且需要达到更远距离情形中的放大器。L-com的该款定向天线配有12英寸(30.5厘米)长的预剥连接线,该连接线配置一个N型母头连接器。 L-com的617~2700MHz LCANLP1003对数周期天线具有11dBi的最大增益,用于5G DAS网络,工作频段为:n1,n2,n3,n5,n7,n8,n12,n13,n14,n18,n20,n25,n26,n28,n29,n30,n34,n38,n39,n40,n41,n53,n65,n66,n67,n67,n70,n71,n80,n81,n82,n83,n84,n85,n86,n89,n90,n91,n92,n93,n94,n95,n97,n98。该款配置N型母头连接器的5G定向对数周期天线已备货在库,并可当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持和销售人员,他们将为您热情解答。
    • 1+

      ¥1712.22
    • 200+

      ¥683.19
    • 500+

      ¥660.36
    • 1000+

      ¥649.08
  • 订货
  • 698~960/1710~2700/4900-6000MHz低PIM级吸顶式DAS天线 - N型母头 - HG75805CUPR-NF The HyperLink HG75805CUPR-NF is a low PIM high performance omni-directional ceiling mount antenna specifically designed for in-building wireless networks such as DAS (Distributed Antenna Systems) which are used to distribute Cellular and WiFi signals throughout a building or area. The Ultra-Wide Band design of this antenna eliminates the need to purchase different antennas for each frequency. This simplifies installations since the same antenna can be used for a wide array of in-building wireless applications where wide coverage is desired.

    Complete WiFi Coverage

    The HG75805CUPR-NF is designed to provide complete WiFi coverage from 2400 MHz to 6000 MHz and is compatible with IEEE 802.11a/b/g/n as well as 802.11ac networks. This adds an additional level of wireless coverage rather than using just the 2.4 GHz 802.11b/g bands. In addition, this antenna can operate in the 4.9 GHz band which is typically used with public safety services such as police and first responders. This along with the HG75805CUPR-NF coverage of the cellular/LTE bands makes this antenna ideal for in-building DAS applications.

    Low PIM Rated

    The key to providing the best performance in a DAS application is to ensure the components used are low PIM rated. This helps meet the increasing demand for higher data rates and the ability to provide streaming video for mobile devices. With a low PIM rating of <-153 dBc, the HG75805CU-PR helps meets the most demanding PIM requirem
    • 1+

      ¥1768.5
    • 200+

      ¥705.64
    • 500+

      ¥682.06
    • 1000+

      ¥670.41
  • 订货
  • 698-960/1710-2700 MHz 10 dBi分布式对数周期天线 - N型母头 - HG72710LP-NF The HyperLink HG72710LP-NF is a high performance wide band log periodic antenna designed to operate from 698-960 MHz and 1710-2700 MHz. This Wideband design eliminates the need to purchase different antennas for each frequency. This simplifies installations since the same antenna can be used for a wide array of wireless applications where wide coverage is desired.

    The HG72710LP-NF is ideal for Distributed Antenna Systems, DAS. A DAS system is used to distribute Cellular and WiFi signals throughout a building or area. It is also suited for directional and multipoint IEEE 802.11b/g/n wireless LANs, public wireless hotspot applications and other systems operating in the 2.4GHz ISM band. The broadband characteristics of the antenna enable it to operate over a very wide frequency range. This antenna features 9/10 dBi of gain and a 56°/45° vertical beam width.

    The internal components of this antenna are enclosed within a UV-stable white ABS radome for all-weather operation. It is supplied with a tilt and swivel mast mount kit.

    For additional information and complete sepcifications, click on the Data Sheet link in the Downloads tab.

    • 1+

      ¥1786.13
    • 200+

      ¥712.68
    • 500+

      ¥688.87
    • 1000+

      ¥677.1
  • 订货
  • 2.4 GHz 8 dBi 全向天线 - 12英寸,反极性SMA公头连接器 - HG2408U-RSP HyperGain HG2408U是一款轻巧型高性能全向WiFi天线,专门用于2.4GHz ISM频段。它特别适合要求高增益和大覆盖范围的多点和移动应用。其他应用包括IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?和公共无线热点应用。

    坚固且防风雨

    此款天线在结构上采用耐用的玻璃纤维天线罩,兼具耐用和美观的特性。它的安装系统采用重负荷压铝固定架和不锈钢U形螺栓,强度极佳。

    • 1+

      ¥1816.1
    • 200+

      ¥724.64
    • 500+

      ¥700.42
    • 1000+

      ¥688.46
  • 订货
  • NULL L-com的HG65807XPPR-4310F为一款低PIM级高性能挂壁式MIMO平板天线,专门设计用于DAS(分布式天线系统)等楼内无线网络。L-com的HG65807XPPR-4310F增益为5.5~7dBi,可用于在整栋楼内或整个区域内分布蜂窝信号和WiFi信号。HG65807XPPR-4310F的工作频率为617~6000MHz,极其适合于包括LoRA、LTE-M及NB-IOT在内的5G、 LTE、CDMA、LPWAN/IoT/M2M应用。HG65807XPPR-4310F天线的多频段设计使得单个天线能够满足多种需要宽覆盖的楼内无线用途需求,从而实现免于为每一频率分别购置不同的天线且使得安装更为简单的优点。 L-com的HG65807XPPR-4310F具有60度的方向性图案,具有+/-45倾斜极化,并具有4.3-10型连接器。在电信行业中,实现最佳性能的关键一点在于,确保所使用的部件为低PIM级部件。这一点有助于满足日益增长的高数据速率需求,以及移动设备的视频串流需求。HG65807XPPR-4310F的工作频率为617~6000MHz,额定PIM低至<-150dBc,有助于满足5G与LTE/4G频段最为严苛的PIM要求。 L-com的HG65807XPPR-4310F天线配置N型连接器,专门设计用于楼内使用,极其适合于室内庭院、室内运动场馆、会议中心及购物中心等大型开放区域。随附的安装支架与五金零件使得天线的安装极为简单易行。与L-com种类繁多的其他优质射频产品一样,该款5G蜂窝天线可在订购当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持与销售人员。
    • 1+

      ¥1861.64
    • 200+

      ¥1748.45
    • 500+

      ¥1690.02
    • 1000+

      ¥1661.15
  • 订货
  • 2.4 GHz 8.5 dBi全向天线,标配磁铁吸盘- 10英尺馈线N型公头连接器 - HG2409MGU-NM 高性能
    HyperGain HG2409MGU是高性能全向WiFi天线,它专门用于2.4 GHz ISM频段和2.36 GHz CDMA频段。这款轻巧型天线非常适合IEEE 802.11b、802.11g和802.11n无线局域网、公共无线热点、蓝牙?以及需要高增益和大覆盖范围的其它多点和移动应用。此天线包括磁性基座和10英尺的高性能低损耗195系列线缆,此线缆与N型母头、N型公头或反极性SMA插头连接器端接,另外,由于具有基座,此天线适合台子或移动应用。

    全天候运行
    HG2409MGU适合全天候运行,它的特点是密封同线黄铜元件都在耐用的抗紫外线灰色玻璃纤维天线罩中。排气端盖和底座内的排水孔可以防止湿气在天线内部积聚。由于具有这些特点,HG2409MGU可以在上方或下方安装。具有可选的天线安装支架
    • 1+

      ¥1873.76
    • 200+

      ¥747.64
    • 500+

      ¥722.66
    • 1000+

      ¥710.32
  • 订货
  • 5.1GHz到5.8 GHz, 31 dBi,宽频抛物面天线,集成 N 型母头连接器 - HG5158-31D HyperGain抛物面WiFi天线设计为远距离工作,并具有重型轻质防水结构。
    • 1+

      ¥1886.13
    • 200+

      ¥1771.46
    • 500+

      ¥1712.26
    • 1000+

      ¥1683.01
  • 订货
  • 2.4 GHz 8 dBi全向天线 - 12英寸,反极性TNC公头连接器 - HG2408U-RTP HyperGain HG2408U是一款轻巧型高性能全向WiFi天线,专门用于2.4GHz ISM频段。它特别适合要求高增益和大覆盖范围的多点和移动应用。其他应用包括IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?和公共无线热点应用。

    坚固且防风雨

    此款天线在结构上采用耐用的玻璃纤维天线罩,兼具耐用和美观的特性。它的安装系统采用重负荷压铝固定架和不锈钢U形螺栓,强度极佳。

    • 1+

      ¥1927.8
    • 200+

      ¥769.21
    • 500+

      ¥743.5
    • 1000+

      ¥730.8
  • 订货
  • 380~6000MHz低PIM级吸顶式安防DAS天线 - N型母头 - HG35805CUPR-NF The HyperLink HG35805CUPR-NF is a multi-band low PIM omni-directional ceiling mount antenna specifically designed for in-building wireless networks. With coverage from 380 MHz to 6000 MHz, the HG35805CUPR-NF is ideal for Standard and Public Safety DAS (Distributed Antenna Systems) which are used to distribute Cellular and WiFi signals throughout a building or area. In additional to providing coverage for WiFi and LTE networks, the HG35805CUPR-NF also provides coverage for TETRA and UHF wireless systems. The multi-band design of this antenna eliminates the need to purchase different antennas for each frequency. This simplifies installations since the same antenna can be used for a wide array of in-building wireless applications where wide coverage is desired.

    Complete WiFi Coverage

    The HG35805CUPR-NF is designed to provide complete WiFi coverage from 2400 MHz to 6000 MHz and is compatible with IEEE 802.11a/b/g/n and 802.11ac networks. This adds an additional level of wireless coverage rather than using just the 2.4 GHz 802.11b/g bands. In addition, this antenna can operate in the 4.9 GHz band which is typically used with public safety services such as police and first responders. This along with the HG35805CUPR-NF coverage of the cellular/LTE bands makes this antenna ideal for in-building DAS applications.

    Low Band Coverage

    With operational coverage down to 380 MHz, the HG35805CUPR-NF can provide support for UHF, 600 MHz, 1390-1432 MHz and AWS-3 bands in addition to providing WiFi and LTE coverage all from a single antenna.

    Low PIM Rated

    The key to providing the best performance in a DAS application is to ensure the components used are low PIM rated. This helps meet the increasing demand for higher data rates and the ability to provide streaming video for mobile devices. With a low PIM rating of <-150 dBc, the HG75805CU-PR helps meets the most demanding PIM requirements for LTE/4G bands.

    The aesthetically pleasing design of this antenna makes it ideal for use in almost any indoor environment. It can be easily mounted through a single 1.0 inch hole in a solid or suspended ceiling up to 1.2 inches thick. This antenna features a 12 inch coax lead terminated with an N-Female connector. Special order connectors are also available.

    For additional information and complete specifications, click on the Data Sheet link in Downloads section.

    • 1+

      ¥1960.25
    • 200+

      ¥782.15
    • 500+

      ¥756.02
    • 1000+

      ¥743.1
  • 订货
  • 2.4 GHz 9 dBi桌面式全向天线 - 4.0英尺反极性TNC公头连接器 - RE09U-RTP 此款WiFi天线特别适合需要360度覆盖范围的应用。此款天线采用有利的磁性基座,因而特别适合用于台子或架子上。它可以在室内或户外使用,从而达到对讲机天线或PC卡内置天线双倍的范围。它特别适合IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?、公共无线热点应用以及使用2.4GHz ISM频段和2.36 GHz CDMA频段的其他系统。

    天线采用附带4英尺线缆的磁性基座,这根线缆与相应无线电连接器端接,因而,无需另外使用无线电天线转接器。

    RE09U适合全天候运行,它的特点是密封同线黄铜元件都在耐用的抗紫外线灰色玻璃纤维天线罩中。排气端盖和底座内的排水孔可以防止湿气在天线内部积聚。由于具有这些特点,RE09U可以在上方或下方安装。

    此款天线可以在上方或下方安装并且具有可选天线安装支架。

    可以订购定制连接器。欲了解更多信息,请联系L-com的销售人员。
    • 1+

      ¥2021.71
    • 200+

      ¥806.68
    • 500+

      ¥779.72
    • 1000+

      ¥766.4
  • 订货
  • 5.8 GHz, 8 dBi, WLAN全向天线,集成 N 型母头连接器 - HG5808U HyperlinkOmni天线是非常紧凑且高性能全向WiFi天线,设计用于5.8GHzISM和UNII频段。它们是要求高增益和宽覆盖范围的多点和移动应用的理想选择。
    • 1+

      ¥2030.4
    • 200+

      ¥810.15
    • 500+

      ¥783.07
    • 1000+

      ¥769.7
  • 订货
  • 5.8 GHz,12 dBi,专业级全向天线, 集成 N 型母头连接器 - HG5812U-PRO HyperlinkOmni天线是非常紧凑且高性能全向WiFi天线,设计用于5.8GHzISM和UNII频段。它们是要求高增益和宽覆盖范围的多点和移动应用的理想选择。
    • 1+

      ¥2046.74
    • 200+

      ¥816.67
    • 500+

      ¥789.38
    • 1000+

      ¥775.89
  • 订货
  • 2.4 GHz 9 dBi桌面式全向天线 - 4.0英尺反极性SMA公头连接器 - RE09U-RSP 此款WiFi天线特别适合需要360度覆盖范围的应用。此款天线采用有利的磁性基座,因而特别适合用于台子或架子上。它可以在室内或户外使用,从而达到对讲机天线或PC卡内置天线双倍的范围。它特别适合IEEE 802.11b、802.11g和802.11n无线局域网、蓝牙?、公共无线热点应用以及使用2.4GHz ISM频段和2.36 GHz CDMA频段的其他系统。

    天线采用附带4英尺线缆的磁性基座,这根线缆与相应无线电连接器端接,因而,无需另外使用无线电天线转接器。

    RE09U适合全天候运行,它的特点是密封同线黄铜元件都在耐用的抗紫外线灰色玻璃纤维天线罩中。排气端盖和底座内的排水孔可以防止湿气在天线内部积聚。由于具有这些特点,RE09U可以在上方或下方安装。

    此款天线可以在上方或下方安装并且具有可选天线安装支架。

    可以订购定制连接器。欲了解更多信息,请联系L-com的销售人员。
    • 1+

      ¥2046.74
    • 200+

      ¥816.67
    • 500+

      ¥789.38
    • 1000+

      ¥775.89
  • 订货
  • NULL L-com LCANLP1012是一款高性能宽带对数周期天线,设计用于698至4200 MHz的点对点通信。L-com的LCANLP1012增益为11 dBi,可用于宽频率范围内的远距离定向通信。LCANLP1012是提升5G、LTE、CMDA、LoRA、物联网和WIFI的理想选择。 对数周期天线LCANLP1012具有垂直波束宽度为50度,水平波束宽度为65度。该天线具有垂直极化,附带的安装支架允许垂直或水平安装配置。对数周期天线用作现有蜂窝信号较弱且需要达到更远距离情形中的放大器。L-com定向天线有一根8英寸长的预剥连接线,端接1个N型母头连接器。 L-com的698至4200 MHz对数周期LCANLP1012天线具有11 dBi的最大增益,适用于5G DAS网络,工作频率为:n1、n2、n3、n5、n7、n8、n12、n13、n14、n18、n20、n25、n26、n28、n29、n30、n34、n38、n39、n40、n41、n48、n53、n65、n66、n67、n67、n70、n71、n77、n78、n80、n81、n82、n83、n84、n85、n86、n89、n98、n95、n95、n95、n91、n91、n95、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、N。该款带有 N 型母头连接器的 5G 定向对数周期天线有现货,可在当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持和销售人员,他们将为您热情解答。
    • 1+

      ¥2054.73
    • 200+

      ¥819.85
    • 500+

      ¥792.46
    • 1000+

      ¥778.92
  • 订货
  • 2.4 GHz 8.5 dBi全向天线,标配磁铁吸盘- 10英尺馈线反极性SMA公头连接器 - HG2409MGU-RSP 高性能
    HyperGain HG2409MGU是高性能全向WiFi天线,它专门用于2.4 GHz ISM频段和2.36 GHz CDMA频段。这款轻巧型天线非常适合IEEE 802.11b、802.11g和802.11n无线局域网、公共无线热点、蓝牙?以及需要高增益和大覆盖范围的其它多点和移动应用。此天线包括磁性基座和10英尺的高性能低损耗195系列线缆,此线缆与N型母头、N型公头或反极性SMA插头连接器端接,另外,由于具有基座,此天线适合台子或移动应用。

    全天候运行
    HG2409MGU适合全天候运行,它的特点是密封同线黄铜元件都在耐用的抗紫外线灰色玻璃纤维天线罩中。排气端盖和底座内的排水孔可以防止湿气在天线内部积聚。由于具有这些特点,HG2409MGU可以在上方或下方安装。具有可选的天线安装支架
    • 1+

      ¥2075.34
    • 200+

      ¥828.08
    • 500+

      ¥800.41
    • 1000+

      ¥786.73
  • 订货
  • HyperGain 3.5GHz 11.5 dBi WiMAX全向天线 - HG3512UP-NF HyperGain HG3512UP-NF是一款经济型高性能全向WiFi天线,它专门用于3.5GHz频段,也已经针对这种频段进行优化。典型应用包括IEEE 802.16e、WiMAX和移动WiMAX应用。此款天线特别适合需要大覆盖范围的多点应用。

    HG3512UP-NF在结构上采用灰色玻璃纤维天线罩,兼具耐用和美观的特性。随附的安装系统采用重负荷钢固定架和一对U形螺栓,用于将天线装在直径介于1.4英寸(35mm)和2.0英寸(50mm)的天线杆上。此天线采用集成式N型母头连接器。

    _x005F_x0002_
    • 1+

      ¥2104.4
    • 200+

      ¥839.67
    • 500+

      ¥811.61
    • 1000+

      ¥797.75
  • 订货
  • 5.3 GHz 10 dBi全向无线局域网天线 - HG5310U HyperGain HG5310U是一个紧凑且高性能全向WiFi天线,专门用于提高5.3GHz频段的IEEE 802.11a无线局域网设备的发射距离和覆盖面积。它具有10 dBi的增益,特别适合需要高增益和大覆盖范围的多点和移动应用。

    HG5310U在结构上采用玻璃纤维天线罩,兼具耐用和美观的特性。此款全向天线附带的安装系统采用重负荷钢固定架和U形螺栓,强度极佳。
    • 1+

      ¥2145.05
    • 200+

      ¥855.89
    • 500+

      ¥827.29
    • 1000+

      ¥813.16
  • 订货
  • 2.4 GHz 20 dBi栅格天线,压铸型,带迷你反射器 - N型母头,5件装 - HG2420EG-NF-5PK The HyperLink Directional Reflector Grid WiFi Antenna provides 20 dBi gain with a 12° horizontal beam-width for directional applications. Applications include point to point systems, point to multi-point and wireless bridges in the 2.4GHz ISM band as well as IEEE 802.11b/g/n wireless LAN systems. Its compact design makes it nearly invisible in most installations, and it can be installed for either vertical or horizontal polarization.

    This antenna's construction features a die cast aluminum reflector grid for superior strength. This antenna's 2-piece reflector grid is simple to assemble and significantly reduces shipping costs. The grid surface is UV powder coated for durability and aesthetics. The open-frame grid design minimizes wind loading.

    The HG2420G WiFi antenna is supplied with a 60 degree tilts and swivel mast mount kit. This allows installation at various degrees of incline for easy alignment. It can be adjusted up or down from 0° to 60°.

    Available in Singles
    This antenna is also available in Singles - HG2420EG-NF

    For additional information and complete specifications, see the data sheet in the downloads section.

    • 1+

      ¥2150.41
    • 200+

      ¥858.03
    • 500+

      ¥829.36
    • 1000+

      ¥815.19
  • 订货
  • 2.4 GHz 14 dBi 90°双极性/双馈源扇区天线 - HG2414DP-090 HyperLink HG2414DP-090双极性扇形板状WiFi天线将高增益与大范围的90°波束宽度结合在一起。它是专业级蜂窝基站天线,专门针对2.4GHz频段的服务提供商设计。应用包括IEEE 802.11b、802.11g和802.11n无线局域网系统。

    双极性设计

    天线采用交叉偶极单元的特殊阵列。此天线通过两个N型内螺纹端口接受反馈,一个端口用于垂直极化信号,另一个端口用于水平极化信号。由于具有这些特点,这些天线特别适合极化分集式系统。

    坚固且防风雨

    此款双频段扇形天线采用重负荷玻璃纤维天线罩,适合全天候运行。重负荷安装系统可以在安装时调整向下倾斜角度(0-10度)。

    特别适合无线互联网蜂窝基站

    由于可以通过调整向下倾斜角度轻松确定蜂窝尺寸,此款天线是无线互联网提供商蜂窝基站的理想选择。垂直覆盖为整整90度。

    这种天线成为Ubiquiti AirMax扇形2G-16-90天线的理想替代产品。

    有关其他信息和完整技术规格,请单击下面的数据表链接。

    • 1+

      ¥2175.13
    • 200+

      ¥867.9
    • 500+

      ¥838.89
    • 1000+

      ¥824.56
  • 订货
  • 698~960/1710~2700MHz低PIM级2×2 MIMO吸顶式DAS天线 - N型母头 - HG72706DPCUPR-NF The HyperLink HG72706DPCUPR-NF is a low PIM high performance MIMO ceiling mount antenna specifically designed for in-building wireless networks such as DAS (Distributed Antenna Systems) which are used to distribute Cellular and WiFi signals throughout a building or area. The wide band design of this antenna eliminates the need to purchase different antennas for each frequency. This simplifies installations since the same antenna can be used for a wide array of in-building wireless applications where wide coverage is desired.

    The HG72706DPCUPR-NF features linear radiators, which means the antenna can receive both vertical and horizontal signals. This provides better overall wireless performance since it can receive signals from a wider array of devices in many different orientations. The HG72706DPCUPR-NF is a MIMO antenna. Two separate antenna leads are provided, each having the ability to receive both vertical and horizontal signals equally. This antenna is ideal for use with 1x2 and 2x2 MIMO access points and routers.

    Low PIM Rated

    The key to providing the best performance in a DAS application is to ensure the components used are low PIM rated. This helps meet the increasing demand for higher data rates and the ability to provide streaming video for mobile devices. With a low PIM rating of <-150 dBc, the HG72706DPCUPR-NF helps meets the most demanding PIM requirements for LTE/4G bands.

    The aesthetically pleasing low profile design of th
    • 1+

      ¥2261.75
    • 200+

      ¥902.46
    • 500+

      ¥872.3
    • 1000+

      ¥857.4
  • 订货
  • NULL L-com LCANLP1004 是一款高性能、宽带对数周期天线,设计用于在 600 至 3800 MHz 的频率范围内进行点对点通信。 L-com 的 LCANLP1004 具有 11 dBi 的增益,可用于极宽频率范围内的长距离定向通信。 LCANLP1004 非常适合 5G、LTE、CMDA、LoRA、IoT、WIFI的放大 LCANLP1004对数周期天线 垂直波束宽度为65度,水平波束宽度为85度。该天线为垂直/水平 极化天线,随附的安装支架允许垂直或水平安装配置。对数周期天线用作现有蜂窝信号较弱且需要达到更远距离情形中的放大器。 L-com 定向天线有一个 20 英寸长的预剥连接线,端接 2 个 N 型母头连接器。 L-com 的 600 至 3800 MHz 对数周期 LCANLP1004 天线具有 11 dBi 最大增益,适用于 5G DAS 网络,工作频段为: n1、n2、n3、n5、n7、n8、n12、n13、n14、n18、n20、n25、n26、n28 ,n29,n30,n34,n38,n39,n40,n41,n48,n53,n65,n66,n67,n67,n70,n71,n77,n78,n80,n81,n82,n83,n84,n85,n86,n89 , n90, n91, n92, n93, n94, n95, n97, n98。这款带有 N 母型连接器的 5G 定向对数周期天线有现货,可在当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持和销售人员,他们将为您热情解答。
    • 1+

      ¥2277.36
    • 200+

      ¥2138.9
    • 500+

      ¥2067.42
    • 1000+

      ¥2032.11
  • 订货
  • 5.8 GHz,12 dBi,专业级全向天线, 集成 N 型母头连接器,5件一组 - HG5812U-PRO-5PK HyperlinkOmni天线是非常紧凑且高性能全向WiFi天线,设计用于5.8GHzISM和UNII频段。它们是要求高增益和宽覆盖范围的多点和移动应用的理想选择。
    • 1+

      ¥2340.21
    • 200+

      ¥933.76
    • 500+

      ¥902.56
    • 1000+

      ¥887.14
  • 订货
  • NULL L-com LCANLP1014是一款高性能宽带对数周期天线,设计用于698至6000 MHz的点对点通信。L-com的LCANLP1014具有11 dBi的增益,可用于宽频率范围内的远距离定向通信。LCANLP1014是提升5G、LTE、CMDA、LoRA、物联网和WIFI的理想选择。 对数周期天线LCANLP1014具有垂直波束宽度为50度,水平波束宽度为65度。该天线具有垂直极化,附带的安装支架允许垂直或水平安装配置。对数周期天线用作现有蜂窝信号较弱且需要达到更远距离情形中的放大器。L-com定向天线有一根8英寸长的预剥连接线,端接1个N型母头连接器。 L-com的698至6000 MHz对数周期LCANLP1014天线具有11 dBi的最大增益,适用于5G DAS网络,使用频段为:n1、n2、n3、n5、n7、n8、n12、n13、n14、n18、n20、n25、n26、n28、n29、n30、n34、n38、n39、n40、n41、n46、n47、n48、n53、n65、n66、n67、n70、n71、n77、n78、n79、n80、n81、n82、n83、n84、n41、n96、n96、n95、n95、n95、n95、n95、n95、n95、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、n91、N。该款带有 N 型母头连接器的 5G 定向对数周期天线有现货,可在当天发货。如有天线或L-com其他产品方面的疑问,请联系我们经验丰富的技术支持和销售人员,他们将为您热情解答。
    • 1+

      ¥2948.19
    • 200+

      ¥1176.35
    • 500+

      ¥1137.04
    • 1000+

      ¥1117.62
  • 订货
  • 立创商城为您提供WIFI天线型号、厂家、价格、库存、PDF数据手册、图片等信息,为您购买WIFI天线提供详细信息